Hi,i want to use the pressure sensor MPX5010DP OR MOXV5010DP to monitor the pressure at which a crack develop on the application of the pressure.How do i connect the sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi,i want to use the pressure sensor MPX5010DP OR MOXV5010DP to monitor the pressure at which a crack develop on the application of the pressure.How do i connect the sensor?

2,279 Views
peterugboji
Contributor I

how do i connect the sensor to measure the pressure?

Labels (1)
0 Kudos
Reply
3 Replies

1,538 Views
david_diaz
NXP Employee
NXP Employee

Hello Peter,

In terms of electrical connections for the MPX5010DP, you may refer to the following figure, especially at the pin style:

pressure_sensors.jpg

In terms of Mounting Techniques, you may refer to the following application note:

AN936 - Mounting Techniques, lead forming, and testing of the MPX Series Pressure sensors

Besides, you may refer to the following application note in order to get more information about soldering recommendations:

AN3150 - Soldering Recommendations for pressure sensor devices

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply

1,538 Views
peterugboji
Contributor I

Hi David Diaz,Thanks for your mail,is there anyway you can send me a picture or a Video on how the connection is made please.Thanks.

Peter

0 Kudos
Reply

1,538 Views
david_diaz
NXP Employee
NXP Employee

Hello Peter,

Please accept my apologies if my first answer was not clear.

You may refer to the following post in order to get more information about connecting the MPX5010DP device: 

Different pin styles in pressure sensors documentation. Part 2

Please let me know if, despite this recommendation, you still need more detailed information.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 Kudos
Reply