Hi, do you have an alternative to ABPMJJT015PGAA5 that supports 20 or more PSI, thanks

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hi, do you have an alternative to ABPMJJT015PGAA5 that supports 20 or more PSI, thanks

414 Views
jerome_maye
Contributor I

We’re developing a prototype here  that requires a sensor with the characteristics of the above but with a pressure spec of 20, or more, PSI.

In that regard, I’m looking for alternatives that might suit as any that Honeywell have are back-ordered.

I would be grateful if you could check if NXP stock one such – thank you.

Spec on page 5 page https://sensing.honeywell.com/honeywell-sensing-basic-board-mount-pressure-abp-series-datasheet-2305...  

Labels (1)
0 Kudos
1 Reply

332 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jerome,

First off, thank you for your interest in NXP's pressure sensors!

Looking at the spec, I assume the closest one is the MPX4250DP:

https://www.nxp.com/docs/en/data-sheet/MPX4250D.pdf 

However, it is a completely different package (Unibody, through-hole) and not compatible with liquids. 

For more options, have a look at Differential/Gauge up to 1000 kPa | NXP.

Best regards,

Tomas

0 Kudos