Help me pick an accelerometer

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Help me pick an accelerometer

2,760 次查看
torby
Contributor I

I've been playing with an MMA7660FC, but I think it's not the part I'm looking for. If it is, please correct me :smileywink:

I'm interested in detecting linear motion, and not so much rotational. The main thing I want to know, at least for now, is, "Is the thing going thataway or thisaway?" Of course, playing with the 7660 gives me lots more ideas.

Thanks,

Torby

标记 (1)
0 项奖励
回复
2 回复数

2,433 次查看
Smiffytech
Contributor III

This isn't my area of expertise, so I hope someone will correct me on the physics if I'm wrong: if an object is travelling along a plane at constant velocity, there will be no acceleration to measure. There will have been measurable acceleration to get to that speed, so you should be able to estimate velocity and direction based on PAST data - but there's nothing to measure otherwise, unless the velocity changes. However, if you add a solid-state gyroscope to the equation, when you are moving against the against the axis of the gyro, there is always something to measure.

I don't think I've seen a Freescale accelerometer & gyro in a single device - the only combined sensor I know of is the  FXOS8700CQ, which incorporates an accelerometer with a magnetometer for 6-axis sensing.

So - if you were to grab a Freescale I2C accelerometer, you could also hang something like ST's L3G4200D of the bus too, and work with the combined data. Or use the FXOS8700CQ plus the L3G4200D for 9-axis sensing!

You can get mounted gyros from the likes of Sparkfun and SeeedStudio for prototyping purposes.

Hope this helps!

EDIT: this may help you, but it's way too mathematical for me! https://community.freescale.com/community/the-embedded-beat/blog/2012/03/29/degrees-of-freedom-vs-ax...

0 项奖励
回复

2,433 次查看
torby
Contributor I

Well, yes. In order to know velocity, you integrate acceleration, then don't interpret the results too closely.

0 项奖励
回复