Help me pick an accelerometer

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Help me pick an accelerometer

2,948件の閲覧回数
torby
Contributor I

I've been playing with an MMA7660FC, but I think it's not the part I'm looking for. If it is, please correct me :smileywink:

I'm interested in detecting linear motion, and not so much rotational. The main thing I want to know, at least for now, is, "Is the thing going thataway or thisaway?" Of course, playing with the 7660 gives me lots more ideas.

Thanks,

Torby

タグ(1)
0 件の賞賛
返信
2 返答(返信)

2,621件の閲覧回数
Smiffytech
Contributor III

This isn't my area of expertise, so I hope someone will correct me on the physics if I'm wrong: if an object is travelling along a plane at constant velocity, there will be no acceleration to measure. There will have been measurable acceleration to get to that speed, so you should be able to estimate velocity and direction based on PAST data - but there's nothing to measure otherwise, unless the velocity changes. However, if you add a solid-state gyroscope to the equation, when you are moving against the against the axis of the gyro, there is always something to measure.

I don't think I've seen a Freescale accelerometer & gyro in a single device - the only combined sensor I know of is the  FXOS8700CQ, which incorporates an accelerometer with a magnetometer for 6-axis sensing.

So - if you were to grab a Freescale I2C accelerometer, you could also hang something like ST's L3G4200D of the bus too, and work with the combined data. Or use the FXOS8700CQ plus the L3G4200D for 9-axis sensing!

You can get mounted gyros from the likes of Sparkfun and SeeedStudio for prototyping purposes.

Hope this helps!

EDIT: this may help you, but it's way too mathematical for me! https://community.freescale.com/community/the-embedded-beat/blog/2012/03/29/degrees-of-freedom-vs-ax...

0 件の賞賛
返信

2,621件の閲覧回数
torby
Contributor I

Well, yes. In order to know velocity, you integrate acceleration, then don't interpret the results too closely.

0 件の賞賛
返信