For the FXLN8361 accelerometer, what is the relationship between the BYP pin voltage and the output offsets? I assume it is just 0.5:1. I want to use the BYP pin voltage to change the offset of external amplifiers.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

For the FXLN8361 accelerometer, what is the relationship between the BYP pin voltage and the output offsets? I assume it is just 0.5:1. I want to use the BYP pin voltage to change the offset of external amplifiers.

970件の閲覧回数
carlnelson
Contributor I

For the FXLN8361 accelerometer, what is the relationship between the BYP pin voltage and the output offsets?  I assume it is just 0.5:1.  I want to use the BYP pin voltage to change the offset of external amplifiers.

ラベル(1)
0 件の賞賛
返信
0 返答(返信)