FXOS8700CQ - lnoise

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FXOS8700CQ - lnoise

1,465 次查看
ekalyvio
Contributor II

Hello.

In register  CTRL_REG1 of the FXOS8700CQ acceleration sensor, there is the option lnoise. The manual states the following...

Reduced noise and full-scale range mode (analog gain times 2).
0 – Normal mode
1 – Reduced noise mode; Note that the FSR setting is restricted to ±2 g or ±4 g mode. This feature
cannot be used in ±8 g mode.

When arming that bit at a range of +-2g, is the resolution of  0.244 mg/LSB stays the same or it is being halved (0.122 mg/LSB)?

Does this reduced noise mode has to do anything with oversampling (OSR)?

Thank you very much.

标签 (2)
0 项奖励
回复
1 回复

1,206 次查看
darioarias
NXP Employee
NXP Employee

Hello Efthymios,

According to the datasheet when the full-scale range is set to 2g, the measurement range is –2 g to +1.999 g, and each count corresponds to 0.244 mg at ±14-bits resolution and it's not affected for the low noise mode. Also, the low-noise accelerometer mode works independently of the oversampling modes.

Regards,

Darío

0 项奖励
回复