FXLS9xxx SPI Error due to Asynchronous Timing Discard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FXLS9xxx SPI Error due to Asynchronous Timing Discard

2,141 次查看
mpierpaolo1
Contributor I

Hi,

We are facing an issue, 
implementing an initialization procedure as described in the example in the paragraph "13.4 Example SPI command list" in the NXP application:
"AN12386 SPI Communication Procedure Recommendations for the FXLS9xxxx
Rev. 1.2 — 8 January 2021 Application note"

In detail We receive an error after every attempt of Reading
DEVSTAT and COUNT Register
with Command = 0xC00000D1 

The FXLS response is always 
0x0C0003D4 for each 
Read DEVSTAT and COUNT Register Command = 0xC00000D1 
This means " SPI Error due to Asynchronous Timing Discard" as said in Figure 5 Flow-Chart

We checked SPI: signal integrity and timing all seems OK;
Command seems OK (MSB-first 32 bits) and the FXLS response has CRC correct so 
We are wondering if someone else already faced this issue in the past 
to receive some tips

Thanks and Regards
piero


0 项奖励
回复
2 回复数

2,125 次查看
JozefKozon
NXP TechSupport
NXP TechSupport

Hi Pierpaolo,

please follow the initialization sequence in a file attached. You can also find there an expected outputs. 

With Best Regards,

Jozef

0 项奖励
回复

1,915 次查看
AIRKernel
Contributor I

Hello Jozef ,

We also met this problem.

We followed the commands in this pdf file , but we got the response "0XC0003D4" after sending erery commands.

AIRKernel_0-1688044491717.png

AIRKernel_1-1688044508696.png

That was strange.Please help us to solve this problem .

Best !

0 项奖励
回复