FXLS90322加速度芯片

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXLS90322加速度芯片

11,106 Views
wakaka_
Contributor I

1AN2386手册作为通信手册,指令存在残缺以及存在指令通过手册中的VB程序算出来的CRC8不符合的情况,导致错误,是否有之后的修订版?

2AN12386通信手册中,通过与FXLS90322芯片建立通信的过程中,存在一些软复位以及CRC816bit数据设置指令发送后,回读值不一样的情况(具体表现为第三次的软复位指令以及CRC816 bit指令发送后回读值并非芯片手册回应)是否对后面开发影响有所?

3FXLS90322芯片在开发加速度功能过程中,板子静止时加速度读数在CH0通道下大约是在0x7FD20x7FE2之间的范围内跳动,CH1通道下的加速度数据大约是在0x803B0x804A之间跳动,并非芯片手册上安装位置上的静止读数0g以及-1g,静止状态下的读数在差不多满量程状态下周围变化的情况是一种什么错误吗?通过转动板子换算出来的加速度值大约在1g左右,大体一致,正常静止状态下读数应该为?

#FXLS90322

Labels (2)
0 Kudos
Reply
2 Replies

11,086 Views
guoweisun
NXP TechSupport
NXP TechSupport

Had send to you based on your ticket.

 

 

0 Kudos
Reply

8,828 Views
KKKKK
Contributor I

我遇到了同样的问题,CRC8始终计算不通过。能把资料发我一份吗

0 Kudos
Reply