FXLN8372 Self Test Pin Voltage

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXLN8372 Self Test Pin Voltage

Jump to solution
537 Views
cguarneri
NXP Employee
NXP Employee

Using the FXLN8372QRI with Vdd = 3.3V, will the part be damaged if the Self-Test pin is at 1.5V?

We know the ST pin is specified for logic levels to function correctly; but during the time that the pin is at 1.5V we don’t care what the accelerometer outputs are… we just don’t want to damage the device.

0 Kudos
1 Solution
394 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chris,

Yes, it is outside the specific logic input levels, but not outside the absolute max ratings, so there is no need to worry about the damage.  

Best regards,

Tomas

View solution in original post

0 Kudos
1 Reply
395 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Chris,

Yes, it is outside the specific logic input levels, but not outside the absolute max ratings, so there is no need to worry about the damage.  

Best regards,

Tomas

0 Kudos