FXAS21002C—MISO Pin Question

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXAS21002C—MISO Pin Question

530件の閲覧回数
liben
Contributor I

Hello ,

I encounter a problem when I connect FXLS8471Q and FXAS21002C on the same SPI. The detailed schematic is shown below. Now, the comunication between FXAS21002C and the master is normal. But the comunication between FXLS8471Q and the master is not normal, no matter the FXAS21002C on 3-wire or 4-wire mode. I guess that the MISO pin of FXAS21002C has effect on the MISO pin of FXLS8471Q. The datasheet of FXAS21002C describes that In 4-wire SPI mode the MISO pin is always placed in a high impedance state when CS_B is not asserted (logic high level) and when FXAS21002C is operated in 3-wire SPI mode - bysetting CTRL_REG0[SPIW] = 1 - the SA0/MISO pin is always placed in a high impedance (high-z) state. I want to know how much resistance of the high impedance is.

Best regards,

Ben

pastedImage_1.png

pastedImage_3.png

ラベル(2)
0 件の賞賛
返信
1 返信

333件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hello Ben,

This sounds like a known SPI issue described in the FXAS21002CER including possible workarounds.

Hope it helps.

Best regards,

Tomas

0 件の賞賛
返信