FXAS21002C: HPF and LPF=12.5Hz

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FXAS21002C: HPF and LPF=12.5Hz

879 Views
riscypayne
Contributor I

Hi Is there guideline how to choose or select HPF and LPF function for given application?

I'm using ODR = 12.5Hz and application is directional.

Would HPF reduce the drift or offset readout?

R.

Labels (1)
0 Kudos
Reply
1 Reply

562 Views
anthonyduhamel
NXP Employee
NXP Employee

Hello Rlscy,

LPF cutoff frequency with an 12.5Hz ODR is fixed to 4Hz.

Ftabs.PNG

You can enable the HPF filter by setting the HPF_EN bit in the CTRL_REG0. The HPF filter should remove/attenuate the average value (offset) of the ouput signals.

Anthony

0 Kudos
Reply