FXAS21002 gyro group delay versus ODR and lowpass filter setting

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FXAS21002 gyro group delay versus ODR and lowpass filter setting

ソリューションへジャンプ
2,652件の閲覧回数
jonbrunetti
Contributor I

Hi,

I would like to know the group delay of the FXAS21002C for a given ODR (output data rate) and lowpass filter shown in Table 33 on page 39 of the data sheet. 

For example, at 400Hz ODR, Table 33 has the following entries for the lowpass filter bandwidth:

Table 33. FXAS21002C LPF Cutoff Frequency

BWODR = 400Hz
0b00128
0b0164
0b1x32

The group delay likely increases by 2x for each 2x decrease in the LPF (lowpass filter) cutoff frequency. Also the group delay likely increases by 2x for each 2x decrease in the ODR setting.  Therefore, the group delay for any value in Table 33 would be highly useful.

If the z-transform of the lowpass filter and the sample rate before decimation is known, that would also answer the question.  For example, if a moving average filter is used as the lowpass filter (sometimes called a SINC filter), knowing the sample rate and filter length, prior to decimation to the ODR, would allow the group delay to be calculated.

Thanks in advance for your replies.

Jon

ラベル(1)
0 件の賞賛
返信
1 解決策
2,200件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jon,

Here is the response from the Design team, sorry it has taken so long.

The LPF of the FXAS21002C is a CIC (cascaded integrator-comb) decimator of 2nd order. It has the advantage of down-sampling and filtering lower than the Nyquist rate. This is not a simple moving average filter or sinc.

The group delay of this filter is “N*M-1” samples with N the decimation factor and M the differential delay.

- Knowing that the ADC run at 6400Hz, the decimation factor goes from 8x to 512x (ODR from 6400/800 to 6400/12.5).

- The differential delay is either 1, 2 or 4 for the BW = 00, 01 or 0x respectively.

Thus, group delay = (6400/ODR*M-1)*156.25us.

I hope it helps.

Regards,

Tomas

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,200件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jon,

I just want to inform you that I have requested assistance from our Apps/Design team to clarify your question. I will update this thread once I have their answer.

Regards,

Tomas

0 件の賞賛
返信
2,201件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Jon,

Here is the response from the Design team, sorry it has taken so long.

The LPF of the FXAS21002C is a CIC (cascaded integrator-comb) decimator of 2nd order. It has the advantage of down-sampling and filtering lower than the Nyquist rate. This is not a simple moving average filter or sinc.

The group delay of this filter is “N*M-1” samples with N the decimation factor and M the differential delay.

- Knowing that the ADC run at 6400Hz, the decimation factor goes from 8x to 512x (ODR from 6400/800 to 6400/12.5).

- The differential delay is either 1, 2 or 4 for the BW = 00, 01 or 0x respectively.

Thus, group delay = (6400/ODR*M-1)*156.25us.

I hope it helps.

Regards,

Tomas

0 件の賞賛
返信
2,199件の閲覧回数
jonbrunetti
Contributor I

Thank you for the information.  That is very helpful.

Jon

0 件の賞賛
返信