FRDM-K64F with FRDM-FXS-MULT2-B sensor issue

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

FRDM-K64F with FRDM-FXS-MULT2-B sensor issue

1,050 次查看
ankushgutpa
Contributor I

Hi folk,
i am using

FRDM-K64F board along with FRDM-FXS-MULT2-B sensor board
i have installed frdm sdk v2.3 and running sensor application example demo, but i am not able to initialize and sensor on mult2b board 
ISSDK MAG3110 sensor driver example demonstration with poll mode

 Sensor Initialization Failed 3 
getting above error for every sensor can anyone help is there is any jumper setting is required, or any setting in the software

标签 (1)
0 项奖励
回复
1 回复

846 次查看
shubhadippaul-b
NXP Employee
NXP Employee

Hi Ankush,


Looks like you have wrong I2C Selector Jumpers.

Please ensure that the shunts on jumpers J27 and J28 are at 2-3 position (default).

Please refer to readme.txt included with the project for required Jumper settings.

0 项奖励
回复