FRDM-K64F with FRDM-FXS-MULT2-B sensor issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FRDM-K64F with FRDM-FXS-MULT2-B sensor issue

1,082件の閲覧回数
ankushgutpa
Contributor I

Hi folk,
i am using

FRDM-K64F board along with FRDM-FXS-MULT2-B sensor board
i have installed frdm sdk v2.3 and running sensor application example demo, but i am not able to initialize and sensor on mult2b board 
ISSDK MAG3110 sensor driver example demonstration with poll mode

 Sensor Initialization Failed 3 
getting above error for every sensor can anyone help is there is any jumper setting is required, or any setting in the software

ラベル(1)
0 件の賞賛
返信
1 返信

878件の閲覧回数
shubhadippaul-b
NXP Employee
NXP Employee

Hi Ankush,


Looks like you have wrong I2C Selector Jumpers.

Please ensure that the shunts on jumpers J27 and J28 are at 2-3 position (default).

Please refer to readme.txt included with the project for required Jumper settings.

0 件の賞賛
返信