Does acceleration change the value of the magnet sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does acceleration change the value of the magnet sensor?

1,717 Views
lysco6837
Contributor I

I use fxos8700cq.

Does acceleration change the value of the magnet sensor? 

If acceleration changes the value of the magnet sensor, is there a document that can calibrate it?

Thank You

Labels (2)
Tags (1)
0 Kudos
Reply
1 Reply

1,642 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

No, acceleration should not change the value of the magnet sensing and magnetic change should not cause acceleration sensing.

 

However, when working with magnetometers is important to apply calibration to the sensor to avoid magnetic interference, please find more details in the application note AN4459: https://www.nxp.com/docs/en/application-note/AN4459.pdf

And here is an example code that you can use for the auto-calibration process, you can download it from the following link: https://www.nxp.com/docs/en/application-note-software/AN4459SW.zip

Regards,

Jose

NXP Semiconductors

0 Kudos
Reply