Does acceleration change the value of the magnet sensor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does acceleration change the value of the magnet sensor?

1,726件の閲覧回数
lysco6837
Contributor I

I use fxos8700cq.

Does acceleration change the value of the magnet sensor? 

If acceleration changes the value of the magnet sensor, is there a document that can calibrate it?

Thank You

ラベル(2)
タグ(1)
0 件の賞賛
返信
1 返信

1,651件の閲覧回数
reyes
NXP TechSupport
NXP TechSupport

Hi,

No, acceleration should not change the value of the magnet sensing and magnetic change should not cause acceleration sensing.

 

However, when working with magnetometers is important to apply calibration to the sensor to avoid magnetic interference, please find more details in the application note AN4459: https://www.nxp.com/docs/en/application-note/AN4459.pdf

And here is an example code that you can use for the auto-calibration process, you can download it from the following link: https://www.nxp.com/docs/en/application-note-software/AN4459SW.zip

Regards,

Jose

NXP Semiconductors

0 件の賞賛
返信