Do MPXV5100GC6U can be used as water-pressure sensor ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Do MPXV5100GC6U can be used as water-pressure sensor ?

1,416件の閲覧回数
steventwu
Contributor I

From the datasheet, I can't confirm that this sensor can be used for water-pressure detection .

Do anyone can help me? or it only use for air-pressure detection.

ラベル(1)
0 件の賞賛
返信
1 返信

796件の閲覧回数
miguelsalhuana
NXP Employee
NXP Employee

Steven,

The MPX5100 can be used to measure tank levels by using the column of air method. The sensor will read the change in pressure in the column of air as the tank fills or empties. The sensor is not manufactured to be submerged in water.

Regards,

Miguel

0 件の賞賛
返信