Dimension & notation clarification in FXLN83XXQ

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dimension & notation clarification in FXLN83XXQ

1,617件の閲覧回数
deepakgowda
Contributor I

Hi,

I'm Deepak, i have a doubt in dimension mentioned in page 12 and 15. In the figure "footprint" there are dimensions such as 12X 0.4121, 4X 0.650 etc. I want to know what is 'X' in these dimensions.

ラベル(1)
0 件の賞賛
返信
1 返信

1,511件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Deepak,

The symbol X is used to indicate the number of times the dimension is repeated. The number of repetitions (e.g 12 or 4), followed by the symbol X and a space precedes the dimension text (e.g. 0.4121 or 0.65mm).

I hope it helps.


Regards,

Tomas


PS: If my answer helps to solve your question, please mark it as "Correct" or “Helpful”. Thank you.

0 件の賞賛
返信