Debug with FXTH870902

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Debug with FXTH870902

1,126 次查看
wanminghua
Contributor I

Hi

I'm working with FXTH870902,and I encounter some questions :

No1:

    The variables can not be preserved out of stop1 mode.

     example:.

        Var is a character variable;

        Var equals to  5 in run mode,and then enter into stop1 mode.

 

        if the system is on  ACTIVE BACKGROUND DEBUG mode ,the Var will be preserved after wake up from stop1 mode.But in     normal operation status, the Var will change after wake up from stop1 mode.

  

       What to do? If I need that the Var will  be preserved after wake up from stop1 mode when the system is on normal operation status

 

No2:

  In stop1 mode, how to determine the vehicle is running

 

 

 

 

 

Please help me

thanks

标签 (1)
0 项奖励
回复
0 回复数