Controlling the Sensor Measurement Interface (SMI) in FXTH870911

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Controlling the Sensor Measurement Interface (SMI) in FXTH870911

跳至解决方案
1,253 次查看
TKB
Contributor II

Hi 

Is there a way for me to control the state of the Sensor Measurement Interface (SMI) i.e. turn it OFF or ON when required or is it done by the firmware defined subroutines only?

Exploring this path for additional power savings if possible.

Thanks

Tushar

标记 (1)
0 项奖励
回复
1 解答
1,245 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

This is handled by the TPMS_READ routines: the entire measurement chain is enabled at the beginning of the routine and disabled at the end. So when the program exits the routine, everything has been turned off.

Best regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,246 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

This is handled by the TPMS_READ routines: the entire measurement chain is enabled at the beginning of the routine and disabled at the end. So when the program exits the routine, everything has been turned off.

Best regards,

Tomas

0 项奖励
回复