Controlling the Sensor Measurement Interface (SMI) in FXTH870911

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Controlling the Sensor Measurement Interface (SMI) in FXTH870911

Jump to solution
1,259 Views
TKB
Contributor II

Hi 

Is there a way for me to control the state of the Sensor Measurement Interface (SMI) i.e. turn it OFF or ON when required or is it done by the firmware defined subroutines only?

Exploring this path for additional power savings if possible.

Thanks

Tushar

Tags (1)
0 Kudos
Reply
1 Solution
1,251 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

This is handled by the TPMS_READ routines: the entire measurement chain is enabled at the beginning of the routine and disabled at the end. So when the program exits the routine, everything has been turned off.

Best regards,

Tomas

View solution in original post

0 Kudos
Reply
1 Reply
1,252 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tushar,

This is handled by the TPMS_READ routines: the entire measurement chain is enabled at the beginning of the routine and disabled at the end. So when the program exits the routine, everything has been turned off.

Best regards,

Tomas

0 Kudos
Reply