Consecutive Reads

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Consecutive Reads

跳至解决方案
1,465 次查看
admin
Specialist II

Hi,

I'm using the MPL115A2 over the I2C bus. I need to know if the device supports consecutive read. I.e. If I write the address pointer to 0x00 and send a read command with 4 bytes worth of clock cycles( 4 x 9 clock pulses on the SCL line), will it send me pressure MSB, LSB, temperature MSB, and LSB?

Thanks.

Onkar Raut,

Embedded Systems Engineer,

BNS Solutions, Walpole, MA.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
1,360 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Onkar,

Yes, it will. The MPL115A2 does support a multiple-byte (burst) read.

Regards,

Tomas

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,361 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Onkar,

Yes, it will. The MPL115A2 does support a multiple-byte (burst) read.

Regards,

Tomas

0 项奖励
回复