Hi Tilman,
Yes, as you can notice in the datasheet (Table 3), the offset can be anywhere between 0.75V and 1.25V.
The sensitivity is 1V/kPa, so I would recommend to use the following formula:
Vout = P + 1.2 => The max pressure the sensor will be able to measure is about 3.8 kPa.
Best regards,
Tomas