Confirmation for ESD Damage immunity of MMA8452.

cancel
Showing results for 
Search instead for 
Did you mean: 

Confirmation for ESD Damage immunity of MMA8452.

336 Views
yosukeohkuma
Contributor I

Hi All,

I would like to know about the ESD Damage immunity which is Machine Model as follows the product.

In datasheet, HBM(Human body) and CDM(Charge device) is described. But MM(Machine Model) is not.

MMA8452QR1

I appreciate if you help for this question.

Best Regards,

Yosuke

Labels (1)
0 Kudos
1 Reply

169 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Yosuke Ohkuma,

MM is superseded by CDM.  if you are covered under HBM and CDM, MM is covered.

That is the reason behind MM not present in the datasheet.

http://www.jedec.org/sites/default/files/The_Machine_Model__JC14%203Version_Final_October2012.pdf

As you can find in the link above, use of MM is now outdated.  Only HBM and CDM are only used for ESD per article shown above, therefore it is unnecessary to be shown on the datasheet.


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos