Component and via clearance around Freescale QFN packages

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Component and via clearance around Freescale QFN packages

996 Views
markwilliams
Senior Contributor I

Hi,

We are using a Freescale MMA8452Q accelerometer in our design. The layout guidelines (AN4077) have the following recommendations that I would like clarification on:

  • Do not place any components or vias at a distance less than 5 mm from the package land area. This may cause additional package stress if it is too close to the package land area.


  • Signal traces connected to pads are as symmetric as possible. Put dummy traces on NC pads in order to have same length of exposed trace for all pads.

In the same application guide is a photo of the Freescale demo board which appears to violate these recommendations having vias immediately around the package as well as a decoupling capacitor:

MMA.png

My question is - how essential is the clearance for vias and components to the MMA8452Q? Ideally I would like the decoupling closer than 5mm to the device. Also what is the mechanism for 'causing package stress' if a capacitor is within 5mm of the QFN?

Also, do I really need to put dummy traces on the NC pads?

Thanks, Mark

Labels (1)
Tags (2)
0 Kudos
Reply
3 Replies

585 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Mark,

This device is sensitive to board mounting, the mentioned recommendations were developed to minimize the offset errors, however, these are not critical.

You can place decoupling capacitor closer than 5mm to the device without a problem, under normal conditions, this should not cause any package stress.

And no, you do not really have to put dummy traces on the NC pads.

Regards,

Jose

0 Kudos
Reply

585 Views
markwilliams
Senior Contributor I

Thank you for your reply. I will move my decoupling closer to the IC now.

You mentioned 'offset errors' - what do you mean by this?

Thanks, Mark

0 Kudos
Reply

585 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Mark,

One of the leading sources of error in an accelerometer is attributed to the 0g-offset or bias error, which is defined as “the difference between the measured value of the sensor from the true zero value”, this is what I meant with “offset error”.

You can find how to deal or calibrate this offset error in the following application note: http://cache.freescale.com/files/sensors/doc/app_note/AN4069.pdf

Regards,

Jose

0 Kudos
Reply