Common-mode pressure

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,719件の閲覧回数
jcd
Contributor I

Hello all,

The datasheet of the MPXV7002 does not mention a maximum common mode pressure for the differential sensor.
I need to measure a tiny difference between two sources that are at 2.5bar absolute pressure.
Can the sensor withstand in this situation?

Cheers,

Jean

ラベル(1)
0 件の賞賛
返信
1 解決策
2,248件の閲覧回数
Joshevelle
Senior Contributor I

Hello Jean,

The MPXV7002 has a maximum common mode pressure of 75kPa (~0.75Bar), this value is shown in page 3, Table 2 of the datasheet:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV7002.pdf

Unfortunately we do not have a pressure sensor with +-2kPa pressure range and a maximum common mode of 250kPa (2.5Bar).

The closest recommendation would be the MPXV7025DP, which has a pressure range of +-25kPa and can support up to 200Kpa (2Bar):

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV7025.pdf

The problem here is that you’re trying to measure a small differential pressure between a huge common mode pressure (125x the range), most of our devices can support up to ~5x its pressure range (depending on the package).

We’re sorry we do not have better fit for your application, please let me know if we can help any further.

Hope it helps.

Josh

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,249件の閲覧回数
Joshevelle
Senior Contributor I

Hello Jean,

The MPXV7002 has a maximum common mode pressure of 75kPa (~0.75Bar), this value is shown in page 3, Table 2 of the datasheet:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV7002.pdf

Unfortunately we do not have a pressure sensor with +-2kPa pressure range and a maximum common mode of 250kPa (2.5Bar).

The closest recommendation would be the MPXV7025DP, which has a pressure range of +-25kPa and can support up to 200Kpa (2Bar):

http://cache.freescale.com/files/sensors/doc/data_sheet/MPXV7025.pdf

The problem here is that you’re trying to measure a small differential pressure between a huge common mode pressure (125x the range), most of our devices can support up to ~5x its pressure range (depending on the package).

We’re sorry we do not have better fit for your application, please let me know if we can help any further.

Hope it helps.

Josh

0 件の賞賛
返信
2,248件の閲覧回数
jcd
Contributor I

Dear Josh,

Thank you for the clarification about the value in the datasheet.

Unfortunately the measuring range of the MPXV7025 would result in a too low resolution.

Best regards,

  Jean

0 件の賞賛
返信
2,248件の閲覧回数
Joshevelle
Senior Contributor I

Jean,

You're very welcome. Unfortunately we do not have a 2kPa pressure sensor that can support up to 250kPa. We're sorry for the inconveniences.

Josh

0 件の賞賛
返信