Cavity volume of MPL115A2

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Cavity volume of MPL115A2

1,169件の閲覧回数
ruppert
Contributor I

I am interested in the inherent cavity volume of the MPL115A2 barometric pressure sensor.

Could you please tell me the volume?

thanks,

Best regards

ラベル(1)
タグ(1)
0 件の賞賛
返信
2 返答(返信)

1,071件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Felix,

Thank you for the patience. I just received confirmation from the product engineer and, unfortunately, we do not have such information available. I apologize the inconvenience that this may cause.

Have a great day,

Paulina

0 件の賞賛
返信

1,071件の閲覧回数
lisettelozano
NXP Employee
NXP Employee

Hello Felix,

As per this kind of information is not characterized in any documentation, I’ve contacted the product engineer and waiting for feedback on this. This can take some time; I’ll get back to you as soon as possible.


Have a great day,

Paulina
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信