Can you use liquid solder mask to protect the MPXM2202A pressure sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can you use liquid solder mask to protect the MPXM2202A pressure sensor?

1,293 Views
randymaruschock
Contributor I

I have boards with the MPXM2202A pressure sensor that need to be conformally coated.  If I use liquid solder mask to protect the pressure port of the MPXM2202A, will the liquid solder mask be at risk of damaging the sensor?

here's a link to the product I plan on using.

techspray.com - Wondermask P Peelable Solder Mask 

Regards,

Randy

Labels (1)
0 Kudos
Reply
2 Replies

1,129 Views
miguelsalhuana
NXP Employee
NXP Employee

Randy,

Since the solder mark is a liquid you can't control if it enters the vent hole and damages the sensing membrane.  Our recommendation is to cover the vent hole with something like Kapton tape. This will protect the membrane and can be applied prior to the conformal coating. 

Regards,

Miguel

1,129 Views
randymaruschock
Contributor I

Thank you for the quick response.

0 Kudos
Reply