Can we use MPXx6115 as altimeter sensor?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can we use MPXx6115 as altimeter sensor?

1,100 Views
taodeng
Contributor I

The MPXx6115 max press error is 1.5Kpa, we want use it for barometer .The precision of barometer is no bigger than 1 meter.

Can we use it ?

0 Kudos
Reply
1 Reply

907 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tao,

Please take a look at this thread with a similar topic.

Have you considered using the MPL3115A2? It allows direct altitude reading (almost no additional computing needed) over the I2C interface and offers an altitude resolution down to 30 cm (with max oversampling enabled) with a relative accuracy of ±0.1 kPa (±8 m). For more information please refer to the AN4528 and the example code is available here

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 Kudos
Reply