Can we use MPXx6115 as altimeter sensor?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Can we use MPXx6115 as altimeter sensor?

966件の閲覧回数
taodeng
Contributor I

The MPXx6115 max press error is 1.5Kpa, we want use it for barometer .The precision of barometer is no bigger than 1 meter.

Can we use it ?

0 件の賞賛
返信
1 返信

773件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Tao,

Please take a look at this thread with a similar topic.

Have you considered using the MPL3115A2? It allows direct altitude reading (almost no additional computing needed) over the I2C interface and offers an altitude resolution down to 30 cm (with max oversampling enabled) with a relative accuracy of ±0.1 kPa (±8 m). For more information please refer to the AN4528 and the example code is available here

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

0 件の賞賛
返信