Can I use SensorFusion library with QN9080 or KW-41Z

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can I use SensorFusion library with QN9080 or KW-41Z

636 Views
haarism19
Contributor I

I looked over the Sensor fusion library and its documentation and it shows that it supports FRMD-K22F and FRMD-K64F. The SDK of LPCXPRESSO54114 also shows that it supports sensor fusion library. 

But I wanted to use the sensor fusion libraries with the nxp BLE modules like QN9080 or KW41Z, but the SKDs of these MCU doesn't have any sensor fusion library. In the documentation, it is written that the sensor fusion library is portable and If its possible then how did I achieve it, I'm new to this so any kind of guidance would be helpful. 

Labels (1)
0 Kudos
0 Replies