CAD/Eagle file for MMA8652FC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAD/Eagle file for MMA8652FC?

1,666 Views
kctenpercent
Contributor I

Are there any CAD/Eagle libraries that contain the MMA8652FC?

Thanks,

Ken

Labels (1)
Tags (1)
3 Replies

779 Views
Martin35804
NXP Employee
NXP Employee

Hello,

Find attached the schematic symbols for the MMA8652FC accelerometer in library.

PS: If my answer helps to solve your question, please mark it as “Helpful” or "Correct" . Thank you.

779 Views
fábiovieira
Contributor I

How do I get the MMA8652FC in this file that you put here ?

Thanks, Fabio Vieira

0 Kudos

779 Views
reyes
NXP TechSupport
NXP TechSupport

Hi Fabio Vieira,

You can download the .olb file that Martin35804 attached in the last mail, this file extension is the library for the symbol of the MMA8652FC intended to be used for Allegro/OrCAD and it’s the official Freescale symbol design.

Now if you want to use a different Schematic/Layout editor, there is also an unofficial library for Freescale Sensors for Eagle Schematic/Layout Editor that includes Schematic Symbols and Footprints for Layout, in this library you can find the files for the MMA8652FC. You can download these mentioned library named "Freescale_Sensors_v2.lbr" from the following link: https://community.freescale.com/docs/DOC-103424

You can find also a breakout board design files for the MMA8652FC in the following link in case you are interested: https://community.freescale.com/docs/DOC-103427


Have a great day,
Jose Reyes

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos