Broken download link "GUI Software for Magnetic Rotary Encoder Reference Design"

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Broken download link "GUI Software for Magnetic Rotary Encoder Reference Design"

7,016件の閲覧回数
kyoungshikkang
Contributor I

I bought the "RD-KL46Z-MRE: Magnetic Rotary Encoder Reference Design".

I will test, but can not download the  "GUI Software for Magnetic Rotary Encoder Reference Design".

Please check and inform me how to down this Software.

0 件の賞賛
返信
9 返答(返信)

6,752件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello Kyoungshik,

We are sorry for the convenience. I will check this with the web team to fix the issue.

Meanwhile, I have attached the latest revision of the GUI I have to this post. If you have any issue with, do not hesitate to ask!

Regards,

Anthony

0 件の賞賛
返信

6,751件の閲覧回数
kyoungshikkang
Contributor I

Hello Anthony,

Thanks for your helps.

However, your attached file is not run on the Windows 7, 10 with below message.

message.JPG

Pls more check it.

Regards,

Kyoungshik

0 件の賞賛
返信

6,751件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello Kyounshik,

I would appreciate if you can translate the error message to english. Is is important to expend the message by clicking on

pastedImage_1.png.

Once you give me the right information, I could try to fix the issue.

Regards,

Anthony

0 件の賞賛
返信

6,752件の閲覧回数
kyoungshikkang
Contributor I

Hello Anthony,

Below is extended message.

capture.JPG

Problem signature:
  Problem Event Name: CLR20r3
  Problem Signature 01: magnetic rotary encoder gui.exe
  Problem Signature 02: 3.4.0.0
  Problem Signature 03: 5819e34b
  Problem Signature 04: Magnetic Rotary Encoder GUI
  Problem Signature 05: 3.4.0.0
  Problem Signature 06: 5819e34b
  Problem Signature 07: 9c
  Problem Signature 08: 44
  Problem Signature 09: System.NullReferenceException
  OS Version: 6.1.7601.2.1.0.256.1
  Locale ID: 1042
  Additional Information 1: 1139
  Additional Information 2: 11390e4467927538beca19e6323dba42
  Additional Information 3: fa7a
  Additional Information 4: fa7a8b876e88322e99f4f08cb713d851

Read our privacy statement online:
  http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

If the online privacy statement is not available, please read our privacy statement offline:
  C:\Windows\system32\en-US\erofflps.txt

Regards,

Kyoungshik

0 件の賞賛
返信

6,751件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello Kyoungshik,

Thanks for the message. 

I need to localize the place in the source code where the error occurs on your computer. On my pc I don't see any issue at all; it may come from the system language. We never try the GUI on a Korean computer.

So I have generated for you a software debug revision with some additional message. You just need to copy the attached file at the NXP Magnetic Rotary Encoder software path (could be something like that: C:\Program Files (x86)\NXP\NXP Magnetic Rotary Encoder) and launch the .exe file. Let me know if you can see some pop-up and which one.

 

Thanks,

Anthony

0 件の賞賛
返信

6,751件の閲覧回数
kyoungshikkang
Contributor I

Hello Anthony,

I got the same message.

Capture1.JPG

Problem signature:
  Problem Event Name: CLR20r3
  Problem Signature 01: PKEBMICR10FCFYTS1R10K4RCKFN205HV
  Problem Signature 02: 3.4.0.0
  Problem Signature 03: 5a5f1abf
  Problem Signature 04: Magnetic Rotary Encoder GUI
  Problem Signature 05: 3.4.0.0
  Problem Signature 06: 5a5f1abf
  Problem Signature 07: 9c
  Problem Signature 08: 44
  Problem Signature 09: System.NullReferenceException
  OS Version: 6.1.7601.2.1.0.256.1
  Locale ID: 1042
  Additional Information 1: 1139
  Additional Information 2: 11390e4467927538beca19e6323dba42
  Additional Information 3: fa7a
  Additional Information 4: fa7a8b876e88322e99f4f08cb713d851

Read our privacy statement online:
  http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

If the online privacy statement is not available, please read our privacy statement offline:
  C:\Windows\system32\en-US\erofflps.txt

Do you need to install other programs before installing this program?

Could you send me the original source if possible?

I can debug.

Regards,

Kyoungshik

0 件の賞賛
返信

6,751件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello Kyoungshik,

It is normal to have the error again, as I didn't identify the issue. But I added some pop-up in the execution like below to have a trace:

pastedImage_1.png

Can you check if you have installed the .NET Framework package 4.0?

Download Windows Vista SP2, Windows 7 SP1, Windows 8, Windows 8.1, Windows Server 2008 SP2, Windows ... 

pastedImage_4.png

Regards

Anthony

0 件の賞賛
返信

6,751件の閲覧回数
kyoungshikkang
Contributor I

Hello Anthony,

I got the same result after installing .NET Framework package.

Capture2.JPG

Problem signature:
  Problem Event Name: CLR20r3
  Problem Signature 01: Magnetic Rotary Encoder GUI.exe
  Problem Signature 02: 3.4.0.0
  Problem Signature 03: 5819e34b
  Problem Signature 04: Magnetic Rotary Encoder GUI
  Problem Signature 05: 3.4.0.0
  Problem Signature 06: 5819e34b
  Problem Signature 07: 9c
  Problem Signature 08: 38
  Problem Signature 09: System.NullReferenceException
  OS Version: 6.1.7601.2.1.0.256.1
  Locale ID: 1042
  Additional Information 1: ed25
  Additional Information 2: ed251a9fce7b451e836b62bb1e792f98
  Additional Information 3: 87e0
  Additional Information 4: 87e088830f594b298b8baf74cc9d42f1

Read our privacy statement online:
  http://go.microsoft.com/fwlink/?linkid=104288&clcid=0x0409

If the online privacy statement is not available, please read our privacy statement offline:
  C:\Windows\system32\en-US\erofflps.txt

Please give me a solution to test the  "Magnetic Rotary Encoder Reference Design".

Regards,

Kyoungshik

0 件の賞賛
返信

6,751件の閲覧回数
anthonyduhamel
NXP Employee
NXP Employee

Hello Kyougshik,

The board has an integrated LCD so you could test the board and run the demo without using the software.

Please send me an email at anthony.duhamel(at)nxp.com, I will send you the source code of the GUI, then you should be able to launch the debug with VisualStudio.

Regards,

Anthony

0 件の賞賛
返信