BLOOD PRESSURE MONITOR -mpx5050

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

BLOOD PRESSURE MONITOR -mpx5050

2,408 次查看
jagannathang
Contributor II

we would like to know the following.

1.  HOW TO CONNECT THE VALVE TO MPX5050

2. WHAT IS THE SPECIFICATION OF VALVE FOR THE DEVICE

3.  SPECIFICATON OF CUFF TO BE CONNECTED TO THE MPX5050

4.  HOW DOES AIR IS PUMPED INTO THE CUFF.

0 项奖励
回复
2 回复数

2,042 次查看
david_diaz
NXP Employee
NXP Employee

Hello,

In order to get more information about the hose applications, you may refer to the following application note:

AN1513 - Mounting Techniques and Plumbing Options

I would recommend you to use a smaller hose inside diameter tube, ~0.5mm less than the sensors outside diameter would work.

If you follow the recommendation mentioned before, you just have to push the tube to the port.

Besides, I would like to recommend the Application Note AN1571 - Digital Blood Pressure Meter.

This application note describes a Digital Blood Pressure Meter concept which uses an integrated pressure sensor, analog signal-conditioning circuitry, microcontroller hardware/software and a liquid crystal display.

I hope this information will be useful for you.

If I misunderstood your question, feel free to let me know.  I will be glad to help.

Have a great day.

David Diaz.

Note: If this post answers your question, please click the Correct Answer button. Thank you!

0 项奖励
回复

1,559 次查看
karamchand2188
Contributor I

Hi David,

 

Pls share your e-mail id for more discussion on BP Meter.

We are interested to manufacturer the same.

 

Thanks and Regards

Karam Chand 

Email: karam.chand@wrig.in

 

 

 

0 项奖励
回复