Occasionally, we will see the i2c line lock up on our board which essentially bricks the board. There are two other devices that could be causing this, but I am wondering if there are any conditions where the MPL3115A2 might hold the i2c lines down. And if so, if there is any way to reset or unlock it? For example, toggling one of the i2c lines or sending a special command.