Amperage of MXP5100

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,678件の閲覧回数
sarahd
Contributor II

What is the power consumption of the MXP5100DP?

ラベル(1)
0 件の賞賛
返信
1 解決策
1,667件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sarah,

As shown in the data sheet, the MPX5100DP draws a maximum of 10mA.

Table 4.JPG

Considering the supply voltage of 5V, the max. power consumption is 5V x 10mA = 50mW.

Best regards,

Tomas

元の投稿で解決策を見る

2 返答(返信)
1,668件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Sarah,

As shown in the data sheet, the MPX5100DP draws a maximum of 10mA.

Table 4.JPG

Considering the supply voltage of 5V, the max. power consumption is 5V x 10mA = 50mW.

Best regards,

Tomas

1,650件の閲覧回数
sarahd
Contributor II

Thank you - I had looked over the datasheet but must have missed that!

0 件の賞賛
返信