Altimeter MPL311A2 sensor for navigation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Altimeter MPL311A2 sensor for navigation

1,228 Views
roromiri
Contributor I

Hi everyone,

i would like to know if Altimeter MPL311A2 sensor is applicable in the vehicle for navigation purposes. How sensitive is this sensor to the temperature changes? does it change much? we may change the temperature inside the vehicle by using the air conditioning system or warming inside. do they affect the performance of this sensor?

thank you very much

roro

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

968 Views
Joshevelle
Senior Contributor I

Hello roro,

tanks for using our community.

The MPL3115A2, has a sensitivity of 0.3m and is temperature compensated from -40°C to 85°C. This is specified in the datasheet Table 2, page 5:

http://cache.freescale.com/files/sensors/doc/data_sheet/MPL3115A2.pdf

Hope it helps.

-Josh

0 Kudos
Reply