Hi,
I'm testing the FXLS8964AF sensor on our custom board and I'm not getting any interrupts on INT1 when I configure my sensor for shake detection.
In a struct named gFxls896xafShakeConfig I have found the following comment but FXLS896xAF_INT_PIN_SEL_SDCD_OT_INT2_DIS is equal to 0x00. Is this a bug or have I missed something?
/* SDCD_WT_ENenabled for INT2 */
Our BT_MODE pin is connected to GND and my intention is to use INT1 as our interrupt pin.
This is our register configuration (pretty much the same as it is explained in AN12004 on page 12):
Register Data
0x15 0x00
0x15 0x02 FSR = 4 g and Standby mode
0x17 0x33 Wake ODR = 400 Hz and Sleep ODR = 400 Hz
0x2F 0x20 Enable X axis only for SDCD OT function
0x30 0xF0
0x31 0x04 Debounce time = 4 × (1/400) = 10 ms
0x33 0xFE
0x34 0xFA
0x35 0x02
0x36 0x05
0x20 0xA0 Enabling DRDY_EN and SDCD_OT_EN
0x21 0x00 Routing DRDY interrupt to INT1 pin
0x15 0x03 FSR = 4 g and ACTIVE = 1
Best regards,
Adde
解決済! 解決策の投稿を見る。
Thanks Tomas.
Hi Adde,
FXLS896xAF_INT_PIN_SEL_SDCD_OT_INT2_DIS set to 0x00 configures INT1 pin for routing SDCD OT interrupt.
You can try following sensor configuration for shake detection:
|
Register Name |
Offset |
Value (to write) |
Description |
|
SENS_CONFIG1 |
0x15 |
0x02 |
FSR = +/-4g and Standby mode |
|
SENS_CONFIG3 |
0x17 |
0x33 |
Wake ODR=400 Hz and Sleep ODR = 400 Hz |
|
SENS_CONFIG4 |
0x18 |
0x21 |
Enable SDCD outside of thresholds event Auto-WAKE/SLEEP transition source enable and INT polarity set to high |
|
SDCD_CONFIG1 |
0x2F |
0x20 |
Enabling SDCD OT for X-axis |
|
SDCD_CONFIG2 |
0x30 |
0xF0 |
Enable SDCD function, Enable Absolute Reference Mode and set OT Debounce counter to clear immediately when threshold criteria is false |
|
SDCD_OT_DBCNT |
0x31 |
0x04 |
Debounce time = 4 for transient detection |
|
SDCD_LTHS_LSB |
0x33 |
0xFF |
Registers 33h and 34h set the OT LOWER threshold. In this example it is set to hex2dec (FAFE) × 1.95 mg/LSB = -2.5 g. |
|
SDCD_LTHS_MSB |
0x34 |
0xFA |
|
|
SDCD_UTHS_LSB |
0x35 |
0x02 |
Registers 35h and 36h set the OT UPPER threshold. In this case it is set to hex2dec (0502) × 1.95mg/LSB = +2.5 g |
|
SDCD_UTHS_MSB |
0x36 |
0x05 |
|
|
ASLP_COUNT_LSB |
0x1E |
0xFF |
Registers 1Eh and 1Fh enable the ASLP function and set the sleep mode transition timer. In this example it is set to hex2dec (07D0) × 2.5 ms (400 Hz Wake ODR) = 5 sec |
|
ASLP_COUNT_MSB |
0x1F |
0x08 |
|
|
INT_EN |
0x20 |
0x01 |
Enabling WAKE_OUT_EN |
|
INT_PIN_SEL |
0x21 |
0x00 |
Routing WAKE_OUT_EN interrupt to INT1 pin |
|
SENS_CONFIG1 |
0x15 |
0x03 |
FSR = +/-4 g and ACTIVE = 1 |
Please try suggested sensor configuration.
Regards,
Amit Purohit.
Thanks Tomas.
Hi Adde,
FXLS896xAF_INT_PIN_SEL_SDCD_OT_INT2_DIS set to 0x00 configures INT1 pin for routing SDCD OT interrupt.
You can try following sensor configuration for shake detection:
|
Register Name |
Offset |
Value (to write) |
Description |
|
SENS_CONFIG1 |
0x15 |
0x02 |
FSR = +/-4g and Standby mode |
|
SENS_CONFIG3 |
0x17 |
0x33 |
Wake ODR=400 Hz and Sleep ODR = 400 Hz |
|
SENS_CONFIG4 |
0x18 |
0x21 |
Enable SDCD outside of thresholds event Auto-WAKE/SLEEP transition source enable and INT polarity set to high |
|
SDCD_CONFIG1 |
0x2F |
0x20 |
Enabling SDCD OT for X-axis |
|
SDCD_CONFIG2 |
0x30 |
0xF0 |
Enable SDCD function, Enable Absolute Reference Mode and set OT Debounce counter to clear immediately when threshold criteria is false |
|
SDCD_OT_DBCNT |
0x31 |
0x04 |
Debounce time = 4 for transient detection |
|
SDCD_LTHS_LSB |
0x33 |
0xFF |
Registers 33h and 34h set the OT LOWER threshold. In this example it is set to hex2dec (FAFE) × 1.95 mg/LSB = -2.5 g. |
|
SDCD_LTHS_MSB |
0x34 |
0xFA |
|
|
SDCD_UTHS_LSB |
0x35 |
0x02 |
Registers 35h and 36h set the OT UPPER threshold. In this case it is set to hex2dec (0502) × 1.95mg/LSB = +2.5 g |
|
SDCD_UTHS_MSB |
0x36 |
0x05 |
|
|
ASLP_COUNT_LSB |
0x1E |
0xFF |
Registers 1Eh and 1Fh enable the ASLP function and set the sleep mode transition timer. In this example it is set to hex2dec (07D0) × 2.5 ms (400 Hz Wake ODR) = 5 sec |
|
ASLP_COUNT_MSB |
0x1F |
0x08 |
|
|
INT_EN |
0x20 |
0x01 |
Enabling WAKE_OUT_EN |
|
INT_PIN_SEL |
0x21 |
0x00 |
Routing WAKE_OUT_EN interrupt to INT1 pin |
|
SENS_CONFIG1 |
0x15 |
0x03 |
FSR = +/-4 g and ACTIVE = 1 |
Please try suggested sensor configuration.
Regards,
Amit Purohit.