关于FXN8361QX轴模拟输出的问题

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

关于FXN8361QX轴模拟输出的问题

ソリューションへジャンプ
1,969件の閲覧回数
yongjunjiang
Contributor I

在使用FXLN8361QX轴输出,在X轴输出端只接0.01u电容,0g时输出电压为0.754V,通过100k电阻接入LM324反相端0g时输出电压降为0.683V。

ラベル(3)
タグ(1)
0 件の賞賛
返信
1 解決策
1,710件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yongjun,

Looking at your schematic, there is basically a voltage divider with the internal 10 kΩ resistor causing this voltage drop. To avoid this, I would suggest using a low input offset rail to rail op amp to act as a buffer.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.

元の投稿で解決策を見る

2 返答(返信)
1,710件の閲覧回数
yongjunjiang
Contributor I

Thank you

0 件の賞賛
返信
1,711件の閲覧回数
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Yongjun,

Looking at your schematic, there is basically a voltage divider with the internal 10 kΩ resistor causing this voltage drop. To avoid this, I would suggest using a low input offset rail to rail op amp to act as a buffer.

I hope it helps.

Regards,

Tomas

PS: If my answer helps to solve your question, please mark it as "Correct". Thank you.