System for environmental noise monitoring, with capacity of data storage at micro sd memory, option of wireless communication with computer and other systems to form a sensor network.
This project consists on the design of a noise pollution level metering system, using a sound sensor board. Its value in the health area lies in prevents ear diseases and other conditions due noise pollution.
The capability to create a sensor network, allows generating a statistical study, as well a more detailed study of the noise propagation patterns or the noise pollution source itself.
The acknowledgment of the noise level enable to know the actions required to decrease this kind of pollution without expose human ear.
It has several source codes: the main folder is that called "SSProyectoSonometro" which contains the three modes of operation. The other folder called "XbeePracticaDataSender" contains the source code for reception and sending data by Zigbee communication.
The video has to be watched with the best quality that Youtube allows for a good viewing.
Muy buen trabajo y muy interesante. Me atrajo el hecho de comunicarlo con otros módulos(Xbee, LCD, microSD) así los datos no se pierden. La interfaz con LabView me gustó.
Muy interesante :smileygrin: