Sensor Fusion 7.00 Preview - Part 1

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Sensor Fusion 7.00 Preview - Part 1

Sensor Fusion 7.00 Preview - Part 1

All,

We are busily working to integrate Version 7.00 of the sensor fusion library into the Kinetis Expert (KEX) ecosystem.  ETA is early August.  I have attached here a preview copy of the user manual for that release.  This is subject to the usual disclaimers: content subject to change, no liability, yada yada yada.  There are a LOT of changes.    These are documented ad nauseum in the user guide.  I've also added a lot of our old blog content into the user guide, as I keep getting requests for them.  Please take a look and give me your feedback.

 

FYI, Here is a sample main() for the new fusion, running on FreeRTOS:

 

/* FreeRTOS kernel includes. */
#include "FreeRTOS.h"
#include "task.h"
#include "queue.h"
#include "timers.h"
#include "event_groups.h"

// KSDK and ISSDK Headers
#include "fsl_debug_console.h"  // KSDK header file for the debug interface
#include "board.h"              // KSDK header file to define board configuration
#include "pin_mux.h"            // KSDK header file for pin mux initialization functions
#include "clock_config.h"       // KSDK header file for clock configuration
#include "fsl_port.h"           // KSDK header file for Port I/O control
#include "fsl_i2c.h"            // KSDK header file for I2C interfaces
#include "Driver_I2C_SDK2.h"    // ISSDK header file for CMSIS I2C Driver
#include "fxas21002.h"          // register address and bit field definitions
#include "mpl3115.h"            // register address and bit field definitions
#include "fxos8700.h"           // register address and bit field definitions

// Sensor Fusion Headers
#include "sensor_fusion.h"      // top level magCal and sensor fusion interfaces
#include "control.h"           // Command/Streaming interface - application specific
#include "status.h"            // Sta:tus indicator interface - application specific
#include "drivers.h"           // NXP sensor drivers OR customer-supplied drivers

// Global data structures
SensorFusionGlobals sfg;                ///< This is the primary sensor fusion data structure
ControlSubsystem controlSubsystem;      ///< used for serial communications
StatusSubsystem statusSubsystem;        ///< provides visual (usually LED) status indicator
PhysicalSensor sensors[3];              ///< This implementation uses three physical sensors
EventGroupHandle_t event_group = NULL;

static void read_task(void *pvParameters);              // FreeRTOS Task definition
static void fusion_task(void *pvParameters);            // FreeRTOS Task definition

/// This is a FreeRTOS (dual task) implementation of the NXP sensor fusion demo build.
int main(void)
{
    ARM_DRIVER_I2C* I2Cdrv = &I2C_S_DRIVER_BLOCKING;       // defined in the <shield>.h file

    BOARD_InitPins();                   // defined in pin_mux.c, initializes pkg pins
    BOARD_BootClockRUN();               // defined in clock_config.c, initializes clocks
    BOARD_InitDebugConsole();           // defined in board.c, initializes the OpenSDA port

    I2Cdrv->Initialize(NULL);                                 // Initialize the KSDK driver for the I2C port

    I2Cdrv->Control(ARM_I2C_BUS_SPEED, ARM_I2C_BUS_SPEED_FAST);      // Configure the I2C bus speed

    initializeControlPort(&controlSubsystem);                           // configure pins and ports for the control sub-system
    initializeStatusSubsystem(&statusSubsystem);                        // configure pins and ports for the status sub-system
    initSensorFusionGlobals(&sfg, &statusSubsystem, &controlSubsystem); // Initialize sensor fusion structures
    // "install" the sensors we will be using
    sfg.installSensor(&sfg, &sensors[0], FXOS8700_I2C_ADDR, 1, (void*) I2Cdrv, FXOS8700_Init,  FXOS8700_Read);
    sfg.installSensor(&sfg, &sensors[1], FXAS21002_I2C_ADDR, 1, (void*) I2Cdrv, FXAS21002_Init, FXAS21002_Read);
    sfg.installSensor(&sfg, &sensors[2], MPL3115_I2C_ADDR, 2, (void*) I2Cdrv, MPL3115_Init, MPL3115_Read);
    sfg.initializeFusionEngine(&sfg);         // This will initialize sensors and magnetic calibration

    event_group = xEventGroupCreate();
    xTaskCreate(read_task, "READ", configMINIMAL_STACK_SIZE, NULL, tskIDLE_PRIORITY + 2, NULL);
    xTaskCreate(fusion_task, "FUSION", configMINIMAL_STACK_SIZE, NULL, tskIDLE_PRIORITY + 1, NULL);

    sfg.setStatus(&sfg, NORMAL);                // If we got this far, let's set status state to NORMAL
    vTaskStartScheduler();                      // Start the RTOS scheduler
    sfg.setStatus(&sfg, HARD_FAULT);            // If we got this far, FreeRTOS does not have enough memory allocated
    for (;;) ;
}

static void read_task(void *pvParameters)
{
    uint16_t i=0;                       // general counter variable
    portTickType lastWakeTime;
    const portTickType frequency = 1;   // tick counter runs at the read rate
    lastWakeTime = xTaskGetTickCount();
    while (1)
    {
        for (i=1; i<=OVERSAMPLE_RATE; i++) {
            vTaskDelayUntil(&lastWakeTime, frequency);
            sfg.readSensors(&sfg, i);              // Reads sensors, applies HAL and does averaging (if applicable)
        }
        xEventGroupSetBits(event_group, B0);
    }
}

static void fusion_task(void *pvParameters)
{
    uint16_t i=0;  // general counter variable
    while (1)
    {
        xEventGroupWaitBits(event_group,    /* The event group handle. */
                            B0,             /* The bit pattern the event group is waiting for. */
                            pdTRUE,         /* BIT_0 and BIT_4 will be cleared automatically. */
                            pdFALSE,        /* Don't wait for both bits, either bit unblock task. */
                            portMAX_DELAY); /* Block indefinitely to wait for the condition to be met. */

        sfg.conditionSensorReadings(&sfg);  // magCal is run as part of this
        sfg.runFusion(&sfg);                // Run the actual fusion algorithms
        sfg.applyPerturbation(&sfg);        // apply debug perturbation (testing only)

        sfg.loopcounter++;                  // The loop counter is used to "serialize" mag cal operations
        i=i+1;
        if (i>=4) {                         // Some status codes include a "blink" feature.  This loop
                i=0;                        // should cycle at least four times for that to operate correctly.
                sfg.updateStatus(&sfg);     // This is where pending status updates are made visible
        }
        sfg.queueStatus(&sfg, NORMAL);      // assume NORMAL status for next pass through the loop
        sfg.pControlSubsystem->stream(&sfg, sUARTOutputBuffer);      // Send stream data to the Sensor Fusion Toolbox
    }
}

/// \endcode

标签 (1)
附件
无评分
版本历史
最后更新:
‎07-18-2016 03:01 PM
更新人: