Freedom Sensor Toolbox-Community Edition shows only zeroes in the plot data-how to fix it

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Freedom Sensor Toolbox-Community Edition shows only zeroes in the plot data-how to fix it

Freedom Sensor Toolbox-Community Edition shows only zeroes in the plot data-how to fix it

The Freedom Sensor Toolbox-Community Edition GUI (Graphic User Interface) offers quick and easy demonstration and evaluation of the NXP sensors.

The GUI can be downloaded from this link: https://www.nxp.com/design/software/development-software/sensor-toolbox-sensor-development-ecosystem...

NXP sensor demonstration kits compatible with the GUI are available at this link: https://www.nxp.com/design/sensor-developer-resources/sensor-toolbox-sensor-development-ecosystem/ev...

There is an User Guide available, for the Freedom Sensor Toolbox-Community Edition GUI, describing installation, running and also troubleshooting of some common problems with the GUI. Please find the User Guide at this link: https://www.nxp.com/docs/en/user-guide/STBCEUG.pdf

JozefKozon_0-1613982434320.png

 

Figure 1. The Freedom Sensor Toolbox GUI is running correctly, Main Page

When the toolbox is running correctly, after pressing the Stat button, user can observe change in individual axis in the plot,  according to the change of the individual axis on the sensor evaluated. See Figure 1. for an example with the MMA8652 accelerometer.  Note the green mark in the right down corner indicating, that the GUI and kit is working correctly. User can also observe change in Parameter Details in the Register page. See Figure 2.

JozefKozon_1-1613982434515.png

 

Figure 2. The Freedom Sensor Toolbox GUI  is running correctly, Register Page

Some users might come across an issue, where after pressing the start button, the plot in the Main Page of the Toolbox shows only zeroes for all three axis, no matter how the tilt for any of the axis, of the evaluated sensor changes. See Figure 3. Note the red exclamation mark in the right down corner, indicating an issue with the GUI. Although the Parameter Details in the Register Page shows correct values according the change of individual axis on the evaluated sensor. See Figure 4.

JozefKozon_2-1613982434689.png

 

Figure 3. Plot in the Main Page of the GUI shows only zeroes for all three axis

JozefKozon_3-1613982434891.png

 

Figure 4. Parameter Details in the Register Page of the GUI

The issue with the wrong scaling in the Freedom Sensor Toolbox-Community Edition GUI is linked to the local preference and format on the computer.

The GUIs have been designed in Chandler/USA where decimal symbol is a simple point.

In Europe and in some Asian countries, it is usually a comma, hence this can cause issue with the plot.

The workaround to fix the issue with the unresponsive plot in the Main Page of the GUI is to change the decimal point in Windows operational system from comma to point. Follow the instructions according the following Figures.

JozefKozon_4-1613982435060.png

 

Figure 5. In Start menu press the Settings button

JozefKozon_5-1613982435207.png

 

Figure 6. In the Windows Settings choose Time & Language

JozefKozon_6-1613982435993.png

 

Figure 7. In the Time & Language window choose Region following with Additional date, time & regional settings

JozefKozon_7-1613982436069.png

 

Figure 8. In the Clock and Region choose Change date, time or number formats

JozefKozon_8-1613982436141.png

 

Figure 9. In Region window press Additional settings

JozefKozon_9-1613982436208.png

 

Figure 10. In the Customize Format window change the Decimal symbol to point

After changing the Decimal symbol to point, simply turn on the Freedom Sensor Toolbox GUI and the plot will show changes in the individual axis according to the change in tilt of the sensor for individual axis.

Attachments
No ratings
Version history
Last update:
‎02-25-2021 07:34 AM
Updated by: