Accelerometer: FXLN83XX Breakout Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Accelerometer: FXLN83XX Breakout Board

Accelerometer: FXLN83XX Breakout Board

The FXLN83XX is a 3-axis, low-power, low-g accelerometer along with a CMOS signal conditioning and control ASIC in a small 3 x 3 x 1 mm QFN package. The analog outputs for the X, Y, and Z axes are internally compensated for zero-g offset and sensitivity, and then buffered to the output pads. The outputs have a fixed 0 g offset of 0.75 V, irrespective of the VDD supply voltage. The bandwidth of the output signal for each axis may be independently set using external capacitors. The host can place the FXLN83XXQ into a low-current shutdown mode to conserve power.

Here is a Render of the FXLN83XX Breakout Board downloaded from OSH park:

FXLN83xx_Top_Bottom.jpg

Layout Design for this board:

FXLN83xx_Top_Bottom_Copper.jpg

In the attachments section, you can find the Schematic Source File (SCH), Schematic PDF File, Layout Source File (BRD), Gerber Files (GTL, GBL, GTS, GBS, GTO, GBO, GKO, XLN) and BOM files.

  

If you're interested in more designs like this breakout board for other sensors, please go to Freescale Sensors Breakout Boards Designs – HOMEFreescale Sensors Breakout Boards Designs – HOME

ラベル(1)
添付
評価なし
バージョン履歴
最終更新日:
‎02-17-2015 11:16 AM
更新者: