Secure Provisioning SDK (SPSDK)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Secure Provisioning SDK (SPSDK)

Secure Provisioning SDK (SPSDK) is an open-source development kit with its source code released on Github and PyPI. It contains a set of API modules for custom production tool development which requires more advanced secure provisioning flow. SPSDK enables communication with NXP’s microcontrollers for security features configuration, debug authentication, generation of Secure Binary (SB) images, trust provisioning and secure programming, etc.

Where to start?

  • Visit SPSDK landing page for the latest document and software on Github and PyPI.
  • Latest news? View “Announcement” label below
  • Get help or report issues? Visit Github. We centralize code release and support on Github.
ラベル

ディスカッション

ソート順:
We have upgraded SPSDK to 2.0.1 which includes a large scale of changes: elftosb will be replaced by nxpimage nxpcertgen and nxpkeygen will be replaced by nxpcrypto select appropriate family will be done using: -f/–family parameter move towards options for all parameters with an exception to BLHost removal of crypto backends extend dedicated spsdk.crypto module - serve as the de-facto backend of SPSDK module level imports via init files
記事全体を表示
We plan to upgrade SPSDK to 2.0 in the next release which includes a large scale of changes.  Customers are suggested to prepare for the changes before the 2.0 release (end of Sept 2023).  Major changes in 2.0 are: elftosb will be replaced by nxpimage nxpcertgen and nxpkeygen will be replaced by nxpcrypto select appropriate family will be done using: -f/–family parameter move towards options for all parameters with an exception to BLHost removal of crypto backends extend dedicated spsdk.crypto module - serve as the de-facto backend of SPSDK module level imports via init files
記事全体を表示