Hi @kei_odagiri ,
Yes, the range of keyid from 1 to 0x7BFFFFFF is opened to users, but there are cases customers trust provision some secure objects there, and SE05X_OBJID_TP_MASK can be used to prevent deleting such kind of objects accidently , but of course users may adjust SE05X_OBJID_TP_MASK definition according to their requirements.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------