pkcs11-tool generates 2 private keys for keypairgen

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

pkcs11-tool generates 2 private keys for keypairgen

ソリューションへジャンプ
2,263件の閲覧回数
user4
Contributor I

I'm expecting to have a public and a private key pair when I execute pkcs11-tool command with --keypairgen option, but the outputs says generated 2 private keys.

Is that an expected behavior of se050? If not, am I missing something important?

 

<Environment>

platform: Debian (bullseye)

module variant: SE050C1

 

<Outputs>

# pkcs11-tool --module $PKCS11_MODULE --keypairgen --key-type rsa:2048 --label "sss:20202020"
Using slot 0 with a present token (0x1)
smCom :WARN :Invalid conn_ctx
App   :INFO :Using PortName='/dev/i2c-1:0x48' (ENV: EX_SSS_BOOT_SSS_PORT=/dev/i2c-1:0x48)
sss   :INFO :atr (Len=35)
      00 A0 00 00    03 96 04 03    E8 00 FE 02    0B 03 E8 08 
      01 00 00 00    00 64 00 00    0A 4A 43 4F    50 34 20 41 
      54 50 4F 
sss   :WARN :Communication channel is Plain.
sss   :WARN :!!!Not recommended for production use.!!!
Key pair generated:
Private Key Object; RSA 
  label:      sss:20202020
  ID:         20202020
  Usage:      decrypt, sign
  Access:     sensitive, always sensitive
  Allowed mechanisms: RSA-PKCS,SHA1-RSA-PKCS,SHA224-RSA-PKCS,SHA256-RSA-PKCS,SHA384-RSA-PKCS,SHA512-RSA-PKCS,RSA-PKCS-PSS,SHA1-RSA-PKCS-PSS,SHA224-RSA-PKCS-PSS,SHA256-RSA-PKCS-PSS,SHA384-RSA-PKCS-PSS,SHA512-RSA-PKCS-PSS,RSA-PP
Private Key Object; RSA 
  label:      sss:20202020
  ID:         20202020
  Usage:      decrypt, sign
  Access:     sensitive, always sensitive
  Allowed mechanisms: RSA-PKCS,SHA1-RSA-PKCS,SHA224-RSA-PKCS,SHA256-RSA-PKCS,SHA384-RSA-PKCS,SHA512-RSA-PKCS,RSA-PKCS-PSS,SHA1-RSA-PKCS-PSS,SHA224-RSA-PKCS-PSS,SHA256-RSA-PKCS-PSS,SHA384-RSA-PKCS-PSS,SHA512-RSA-PKCS-PSS,RSA-PP

 

ラベル(1)
0 件の賞賛
返信
1 解決策
2,165件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @user4 ,

 

Thanks for the information! I have tied the same with MW ver 4.5.1 , it just works as expected. Maybe you have to update the MW to the latest. Please kindly refer to the following for details.

Kan_Li_0-1714972873727.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
2,242件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @user4 ,

 

May I have the MW version?

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信
2,229件の閲覧回数
user4
Contributor I

Hi Kan,

Thank you for responding.

Unfortunately, I don't know the specific version of MW because this environment was built by another company, but guessing it might be 4.2.0:

# dpkg -L plug-and-trust
/.
/etc
/etc/plug-and-trust
/etc/plug-and-trust/openssl11_sss_se050.cnf
/usr
/usr/lib
/usr/lib/arm-linux-gnueabihf
/usr/lib/arm-linux-gnueabihf/engines-1.1
/usr/lib/arm-linux-gnueabihf/engines-1.1/e4sss.so
/usr/lib/arm-linux-gnueabihf/libsssapisw.so.4.2.0
/usr/lib/arm-linux-gnueabihf/plug-and-trust
/usr/lib/arm-linux-gnueabihf/plug-and-trust/libsss_pkcs11.so
/usr/share
/usr/share/doc
/usr/share/doc/plug-and-trust
/usr/share/doc/plug-and-trust/changelog.Debian.gz
/usr/share/doc/plug-and-trust/copyright
/usr/lib/arm-linux-gnueabihf/libsssapisw.so.4

 

0 件の賞賛
返信
2,166件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @user4 ,

 

Thanks for the information! I have tied the same with MW ver 4.5.1 , it just works as expected. Maybe you have to update the MW to the latest. Please kindly refer to the following for details.

Kan_Li_0-1714972873727.png

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

0 件の賞賛
返信
2,155件の閲覧回数
user4
Contributor I

Hi Kan,

Thank you for the inputs. I've also verified that using the libraries in that version does solve the problem, so will consider to ask the package provider to update the MW.

0 件の賞賛
返信