determine if Platform SCP keys are correct

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

determine if Platform SCP keys are correct

1,286 次查看
fus
Contributor II

I'm using the middleware 3.0.6 and implemented the Patform SCP key rotation example for a SE050C2. This works as desired but when I later try to connect again with the (no longer valid) default keys without selecting the applet "sss_session_open()" returns success and only later commands fail.

"nxScp03_HostLocal_VerifyCardCryptogram()" and "AuthenticateChannel()" both return fail but "sss_session_open()" does not propagate this failure and only a log message "Could not set SCP03 Secure Channel" is output.

Shouldn't "sss_session_open()" fail if the Platform SCP keys provided are wrong?

0 项奖励
回复
1 回复

1,253 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @fus ,

 

Thanks for the report! Our MW team has confirmed this and will fix it in future MW versions. 

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复