Hi.
I'm looking into verifying the signature of the certificate of one of the trust provisioned keys inside the se050. I've read the certificate issued for each of the trust provisioned keys, and they seem to be signed by a CA called "CloudConn-Intermediate-<serial number>-RSA" and "CloudConn-Intermediate-<serial number>-ECC". Where can I get these CA and the rest of the certificate chain for each of the Device Keys?
Thank you very much for your help.
Please kindly refer to 2.6 SE050 Chain of trust certificates from https://www.nxp.com/docs/en/application-note/AN12436.pdf for details.
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------