SE050 with RPi 3 B v1.2 Not Detecting

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SE050 with RPi 3 B v1.2 Not Detecting

3,584 Views
annimbanerjee
Contributor I

 

Need help to understand if this is RPi related issue or if it something to do with.... connection/wiring or pull-ups. I am not sure.

Info:

- Host: Raspberry Pi 3 B 1.2v
- Jumpers Config: default.[Factory Set][J37,J38 OPEN]
- OS: raspios_full_armhf-2021-05-28/2021-05-07-raspios-buster-armhf-full
- Linux raspberrypi 5.10.17-v7+ #1421
- Dev Kit: SE050 ARD Dev Kit.
- I2C: ENABLED
- Remote GPIO: ENABLED

I2C arm baud rate/speed: 

~/>cat /boot/config.txt
dtparam=i2c_arm_baudrate=10000
 Some more commands and output for more info:
~/>i2cdetect -l
i2c-1 i2c bcm2835 (i2c@7e804000) I2C adapter

~/>i2cdetect -F 1
Functionalities implemented by /dev/i2c-1:
I2C yes
SMBus Quick Command yes
SMBus Send Byte yes
SMBus Receive Byte yes
SMBus Write Byte yes
SMBus Read Byte yes
SMBus Write Word yes
SMBus Read Word yes
SMBus Process Call yes
SMBus Block Write yes
SMBus Block Read no
SMBus Block Process Call no
SMBus PEC yes
I2C Block Write yes
I2C Block Read yes

~/> i2cdetect -y 1
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: -- -- -- -- -- -- -- -- -- -- -- -- --
10: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
20: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
30: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
40: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
50: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
60: -- -- -- -- -- -- -- -- -- -- -- -- -- -- -- --
70: -- -- -- -- -- -- -- --

~/> ls -l /dev/i2c-1
crw-rw-rw- 1 root i2c 89, 1 Jul 13 19:15 /dev/i2c-1

$..../simw-top_build/raspbian_native_se050_t1oi2c/bin > ls -l
.
.
-rwxr-xr-x 1 pi pi 28496 Jul 13 09:52 se05x_Minimal
.
.

$..../simw-top_build/raspbian_native_se050_t1oi2c/bin > sudo ./se05x_Minimal /dev/i2c-1
App :INFO :PlugAndTrust_v03.03.00_20210528
App :INFO :Running ./se05x_Minimal
App :INFO :Using PortName='/dev/i2c-1' (CLI)
smCom :ERROR:Failed writing data (nrWritten=-1).

smCom :ERROR: - Error in I2C Write.....
smCom :ERROR:phNxpEseProto7816_SendRawFrame Error phNxpEse_WriteFrame
smCom :ERROR:TransceiveProcess Transceive send failed, going to recovery!
smCom :ERROR:phNxpEseProto7816_Open failed
smCom :ERROR: Failed to Open session
sss :ERROR:SM_Connect Failed. Status 7012
App :ERROR:sss_session_open failed
App :ERROR:ex_sss_session_open Failed
App :ERROR:!ERROR! ret != 0.


 

Wiring Info:

Cable length of 4 wires: > 2.5 inch. Like a generic length female-to-female wire-length.

 

Please, help is needed.

 

Regards

 

Labels (1)
0 Kudos
Reply
3 Replies

3,570 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @annimbanerjee ,

 

We provide the following app note to use SE050 with Raspberry Pi. Please kindly refer to https://www.nxp.com.cn/docs/en/application-note/AN12570.pdf for details.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

3,562 Views
annimbanerjee
Contributor I

Hello,

Will be looking back at this document again in case if I have missed anything in the setup. I Still have not resolved this issue. Once I resolve this, will surely post the solution here.

 

 

Regards

0 Kudos
Reply

3,545 Views
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @annimbanerjee ,

 

Is there any progress on this issue? Looking forward to your reply!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply