SE050 always NACKS on i2c command

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

SE050 always NACKS on i2c command

跳至解决方案
5,360 次查看
badhri_radhakri
Contributor II

Hi Good day, I'm using SE050 as a I2C slave to my I2C Master STM32 board. Every time when i try to initiate a Soft Reset Request, I always get a nack. 

#define SLAVE_ADDR 0x48<<1

uint8_t packet[5] = {  //for soft reset request
            0x5A,             // NAD
            0xCF,             // PCB for reset
            0x00,            // LEN is 0 no INF
            0x37,            // CRC 1
            0x7F             // CRC 2
};   

while (ret = (HAL_I2C_Master_Transmit(&hi2c1, SLAVE_ADDR, packet, sizeof(packet), 100)) != HAL_OK);
HAL_Delay(50);

/* code */

Please help me with if I'm sending the wrong values. The packet values are calculated as per the I2C specs datasheet. As for the CRC I'm using the SE050 Plug Trust's library function.

Thanks!

标签 (1)
标记 (4)
1 解答
5,109 次查看
badhri_radhakri
Contributor II

Thank you. The problem was with the ENA pin on the board. I wasn't paying attention to it's Jumper positions. Now I'm able to make the chip respond to my commands.

Thanks!

在原帖中查看解决方案

6 回复数
5,109 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Hi,

Actually I could not find any obvious wrong in the packet values, maybe you can use some logical analyzer to probe the I2C frame, and check if it meets the spec as below:

pastedImage_1.png

Please kindly refer to https://www.nxp.com/docs/en/user-guide/UM11225.pdf  for more details.

Hope that helps,

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复
5,109 次查看
badhri_radhakri
Contributor II

Hi Kan_Li‌ thanks, I hooked up a logic analyzer and this is how my waveform looks like:
pastedImage_1.png

There is always a NACK after writing the Slave address which in this case is 0x48<<1. 

Could there be any other mistake I'm making ? :smileysad:

Thanks!

0 项奖励
回复
5,109 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Are you using the SE050ARD board? are the jumpers set correctly? Please refer to https://www.nxp.com/docs/en/application-note/AN12395-OM-SE050ARD_hardware_overview.pdf  for details.

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,110 次查看
badhri_radhakri
Contributor II

Thank you. The problem was with the ENA pin on the board. I wasn't paying attention to it's Jumper positions. Now I'm able to make the chip respond to my commands.

Thanks!

4,005 次查看
Exocet
Contributor II

Hello,

 

Can you share the STM32 porting files ?

I will soon start the port and I need a reference to start with.

Many thanks

0 项奖励
回复
5,109 次查看
Kan_Li
NXP TechSupport
NXP TechSupport

Great to know this issue has been fixed on your side. Thanks for the update!

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------